A new and refreshed look for installation cable packaging

May 31, 2023 - 12:00 AM

We renewed the packaging of installation cables. We will use 50% recycled plastic film instead of the current 30%, thereby reducing the use of raw materials. Product information for cables is provided on streamers, the design of which we have also refreshed.

Product information follows the previous logic:

  • The colour of the streamer indicates the cable class according to the Construction Products Regulation:
    • black stands for class E cables,
    • pink stands for class D cables,
    • blue stands for class C cables.
  • At the bottom of the streamer there is another colour-coded line – red marks 1.5 mm² and orange 2.5 mm².
  • The streamer contains information on Estonian, Latvian and Lithuanian standards.
  • The streamer contains additional information on sustainability aspects of production and products. 

The new packaging will reach the wholesalers of electrical equipment during the summer months.