Power Grids

Empower grid enhancement

Our cable solutions are the backbone of the advanced power grids necessary to achieve the energy transition.

The key pillar of the energy transition happening worldwide is the shift from a fossil-fuel based energy mix to cleaner and more sustainable energy sources. Consequently, the integration of energy from such renewable sources requires enhancements of the power grids. Also, with the ever-increasing demand for electricity in the construction, transportation, and industry segments, grid enhancement is perhaps more crucial now than ever before, to accelerating the energy transition towards a net-zero future.

Prysmian power grids help grid operators and utilities, industrial companies, and installers transmit and distribute the energy that powers every aspect of our world. 

We are unmatched in our overall manufacturing and installation capabilities, and have an unwavering commitment to R&D.

We design, produce and install High, Medium and Low Voltage underground cable systems, providing network components, value added engineering as well as asset monitoring solutions and services.

The role of power grids in enabling the energy transition

The EU has committed to cut greenhouse gas emissions by 55% - compared to 1990 - by 2030, a key milestone in reaching climate neutrality in 2050. According to the Commission’s scenarios, this will require renewables to represent 81% of the total EU’s electricity mix. The necessary condition for a complete transition to renewables and their integration into the energy system is a strong and interconnected grid. As a matter of fact, the Commission envisages 1300 GW onshore and offshore wind by 2050 (up from 180 GW today). The on-going electrification processes in residential, transport and industrial applications require a considerable expansion of existing grids. Strong and resilient connections between renewable generation sources and consumption areas are required to manage weather-related variations in energy supply and the integration of different energy sources to balance such fluctuations.  Next-generation grids must be designed to make power infrastructures stronger, more resilient and deliver maximum performance under any circumstances and in any configuration. 

Connect to Lead in Power Grid

According to its new Connect to lead, business strategy Prysmian aims at seizing the opportunities stemming from the structural megatrends shaping the cable industry and become a global cable solution provider. In line with this mission, the Power Grids business unit:

  • supports power grids upgrade with innovative technologies,
  • promotes grids resilience and sustainability,
  • fosters long lasting customer relationships.

Power Grid products

Bare conductor

Bare conductors (HK)

Aerial cable

Aerial cables (AMKA 1KV, EX, PAS-W, CCST-WK, CCST-W)

Power cable

Power cables 1kV (AXPK-PE, AXPK, AXPK-PLUS, ARLC)

Power cable 12kV

Power cables 12kV (AHXAMK-W 6/10(12) KV, AXQJ-RMF PURE 6/10(12) KV and else)

Power cable 12kV

Power cables 24kV (AHXAMK-W 20KV, AXQJ-RMF PURE 12/20(24) KV, NA2XSY 12/20KV and else)

Power cable 36kV

Power cables 36-52kV (AXALJ-TT 18/30(36) KV, NA2XS(F)2Y 18/30KV CPR F, AXLJ-TTCL 26/45(52) kV and else)

Accessories for Power Cables

Discover our high-quality cold-shrink joints, terminations and separable connectors for Medium-Voltage cables.

  • COLDFIT

    COLDFIT terminations are quick and easy to install, offering high reliability and excellent performance for both indoor and outdoor use.

  • ELASCON

    Separable connector for polymeric MV cables. Indoor and outdoor installation. The connector is entirely protected by a watertight conductive envelope connected to earth.

  • ELASPEED COMPACT

    The Elaspeed® coldshrinkable medium voltage straight through joints are designed for fast, easy and reliable installation.

Materials:

Accessories for Cable Mounting

Discover our cable glands, cleats and terminals.

Prysmian Group´s components business unit, based in Wrexham, is the UK´s leading manufacturer of cable support and fixings systems and offers a range that is both comprehensive and diverse. Through many years of industry experience and working closely with our customers, Prysmian Group is able to offer cleats to support and fix all cable types on the market. 

Our range of products includes: 

Materials:

Contact us

Rait Kuhlberg

Selection of projects


Submarine cable installation

Submarine cable between the mainland and Muhu island

Visit / Download
Cable laying

Underground cable lines in Tallinn

Visit / Download
Wind farm construction

Wind farms in the Baltic states

Visit / Download
Railway station in Tallinn

Renovation project of the Lääne-Harju railway line

Visit / Download
Overhead lines

The Vilnius-Neris 330 kV overhead line strengthens the energy security of Lithuania

Visit / Download
Viljandi hospital

Viljandi gets a new and modern hospital

Visit / Download
ShoreLink shore power solution for cruise ships at the Port of Aarhus

We contribute to a greener future of shipping

Visit / Download
Prysmian 330 kV cable

The largest battery park in continental Europe is connected to the network by a 330 kV cable

Visit / Download